Torque Specifications
WARNING |
|---|
|
Hazard of electric shock
All electrical connections must be torqued according to
this table.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
|
Bolt size |
Torque |
|
|---|---|---|
| UPS | Lithium-ion battery cabinet | |
| M4 | — |
1.7 Nm (1.25 lb-ft) |
|
M6 |
5 Nm (3.69 lb-ft) |
5 Nm (3.69 lb-ft) |
|
M8 |
17.5 Nm (12.91 lb-ft) |
14 Nm (10.33 lb-ft) |
|
M10 |
30 Nm (22 lb-ft) |
30 Nm (22.13 lb-ft) |
|
M12 |
50 Nm (36.87 lb-ft) |
46 Nm (33.93 lb-ft) |
WARNING