990-914301A-001

Overview of Board Locations for External Signal Cables

Follow the procedure Route External Signal Cables to the Boards to route the external signal cables to the boards.

Class 2/SELV

Board Terminal Description See
0P6547 J4931, J4932 +24V SELV Connect the Emergency Power Off (EPO)
J4936-J4938 EPO connections
0P6548 J5502-J5505, J5510 Input contacts IN1-IN5 Overview of Input Contacts and Output Relays
J5506 Input contact IN9
J5520-J5525, J5528 Output relays OUT8,9,10
J5527 Kirk key control Signal Cable Connections to the Switchgear (Boards 0P6547, 0P6548, 0P6549)
J5514 UOB lamp control
J5515 MBB lamp control
J5516 SIB lamp control
J5517 SSIB lamp control
J5509 Redundant UOB AUX
0P3643 PBUS1, PBUS2 PBUS PBUS Cable Connections (Board 0P3643)
0P6502   Modbus Modbus Connections (Board 0P6502)

Non-Class 2/Non-SELV

Board Terminal Description See
0P6547 J4939-J4941* Configurable output relays OUT1, OUT2, OUT3 Overview of Input Contacts and Output Relays
0P6549 J5607 MBB Signal Cable Connections to the Switchgear (Boards 0P6547, 0P6548, 0P6549)
J5608 SIB
J5620 SSIB
J5621 UOB
J5622 UIB
J5611, J5612, J5613 External sync - L1, L2, L3 Signal Cables for External Synchronization
J5609 Battery breaker 1 Signal Cable Connections to Classic Battery Cabinets (Boards 0P6547, 0P6549, 0P6552) and Signal Cable Connections to Battery Breaker Cabinet (Boards 0P6547, 0P6548, 0P6549)
J5610 Battery breaker 2
0P6548 J5529 Battery temperature sensor 1
0P6547 J4942, J4943 24V supply 1
J4929, J4930 24V supply 2
J4923 DC shunt trip 1
J4924 DC shunt Trip 2
0P6552 J9019 Battery breaker 3
J9020 Battery breaker 4
J9021 Battery temperature sensor 2
J9022, J9023 24V supply 3
J9024, J9025 24V supply 4
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?