990-55333D-001

Model List

Scalable UPS Models

  • Galaxy VXL UPS, 0 to 1250 kW, 400 V, start-up 5x8 (GVXL0K1250HS)*

  • Galaxy VXL UPS 500 kW scalable to 1250 kW, 400 V, start-up 5x8 (GVXL500K1250HS)

  • Galaxy VXL UPS 625 kW scalable to 1250 kW, 400 V, start-up 5x8 (GVXL625K1250HS)

  • Galaxy VXL UPS 750 kW scalable to 1250 kW, 400 V, start-up 5x8 (GVXL750K1250HS)

  • Galaxy VXL UPS 875 kW scalable to 1250 kW, 400 V, start-up 5x8 (GVXL875K1250HS)

  • Galaxy VXL UPS 1000 kW scalable to 1250 kW, 400 V, start-up 5x8 (GVXL1000K1250HS)

  • Galaxy VXL UPS 1125 kW scalable to 1250 kW, 400 V, start-up 5x8 (GVXL1125K1250HS)

  • Galaxy VXL UPS 1250 kW, 400 V, start-up 5x8 (GVXL1250KHS)

Non-Scalable UPS Models

  • Galaxy VXL UPS 600 kW, not scalable, 400 V, start-up 5x8 (GVXL600K600HS)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?