Batteries
End of Discharge Voltage
Standard VRLA Voltage Levels
Maximum Battery Current
| UPS rating | 500 kW | 600 kW | 625 kW | 750 kW | 875 kW | 1000 kW | 1125 kW | 1250 kW |
|---|---|---|---|---|---|---|---|---|
|
Number of power modules present in the UPS |
4 |
5 |
5 |
6 |
7 |
8 |
9 |
10 |
|
Maximum continuous battery current (A) |
1200 |
1500 |
1500 |
1800 |
2100 |
2400 |
2700 |
3000 |
|
Maximum battery current (A) for 10 minutes |
1272 |
1590 |
1590 |
1908 |
2226 |
2544 |
2862 |
3180 |
|
Maximum battery current for 3 minutes |
1336 |
1670 |
1670 |
2004 |
2338 |
2672 |
3006 |
3340 |
|
Maximum battery current for 1 minute |
1440 |
1800 |
1800 |
2160 |
2520 |
2880 |
3240 |
3600 |