EIO0000004347_01

Federal Communication Commission Radio Frequency Interference Statement - For USA

FCC Radio Interference Information

This product has been tested and found to comply with the Federal Communications Commission (FCC) limits for a Class A digital device, pursuant to Part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a commercial, industrial or business environment. This product generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause or be subject to interference with radio communications. To minimize the possibility of electromagnetic interference in your application, observe the following two rules:

  • Install and operate this product in such a manner that it does not radiate sufficient electromagnetic energy to cause interference in nearby devices.

  • Install and test this product to ensure that the electromagnetic energy generated by nearby devices does not interfere with the operation of this product.

  • Changes or modifications not expressly approved by the party responsible for compliance could void the user's authority to operate this product.

WARNING
ELECTROMAGNETIC / RADIO INTERFERENCE
Electromagnetic radiation may disrupt the operation of this product leading to unintended equipment operation. If electromagnetic interference is detected:
  • Increase the distance between this product and the interfering equipment.
  • Reorient this product and the interfering equipment.
  • Reroute power and communication lines to this product and the interfering equipment.
  • Connect this product and the interfering equipment to different power supplies.
  • Always use shielded cables when connecting this product to a peripheral device or another computer.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?