EIO0000004347_01

Package Contents

Verify all items listed here are present in your package.

NOTE: This product has been carefully packed with special attention to quality. However, should you find anything damaged or missing, please contact your local distributor immediately.
  1. FP6000 Series: 1

  2. Installation gasket: 1 (attached to the product)

  3. Installation fasteners (attached to the product):

    • 4 pieces (for HMIFP6600TMD, HMIFP6500WCD and HMIFP6600WCD)

    • 8 pieces (for HMIFP6700TMD, HMIFP6700WCD, HMIFP6800WCD and HMIFP6900WCD)

  4. DC power connector: 1

  5. USB clamp (Type B): 1 set (1 bracket, 2 screws and 1 tie)

Product Revision and QR Code for Manual

You can identify the product version (PV) from the product label.

You can also check the contents of this manual by using the QR code on the product label. Confirm the location of the QR code below and refer to the manual.

  1. This mark indicates that you can refer to this manual by using the QR code, and that you must use copper wire rated for 75 °C (167 °F) or higher. Refer to Wiring the Power Supply.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?