EIO0000004347_01

Touch Panel

  HMIFP600TMD HMIFP600WCD
Touch panel type Resistive film (analog) Projected capacitive with optimized noise filter
Touch points Multi-touch (two-point touch) Multi-touch (two-point touch)
Touch panel service life 10 million times or more 10 million times or more
Touch mode Not applicable

Standard mode, water detection mode, glove mode

NOTE: For details, refer to Touch Mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?