Precautions for Building into an End-use Product
This product is designed for use on flat surfaces of UL 50/50E, Type 1, Type 4X (indoor use only), Type 12 or Type 13 enclosure.
Mount this product in an enclosure that provides a clean, dry, robust and controlled environment (IP66F, IP67F, UL 50/50E, Type 1, Type 4X [indoor use only], Type 12 or Type 13 enclosure).
The front surface of displays is rated for IP66F, IP67F, UL 50/50E, Type 1, Type 4X (indoor use only), Type 12 and Type 13 enclosure.
| Display front surface | Enclosure front surface |
|---|---|
| IP66F, IP67F, UL 50/50E, Type 1, Type 4X (indoor use only), Type 12, Type 13 | IP66F, IP67F, UL 50/50E, Type 1, Type 4X (indoor use only), Type 12, Type 13 |
When the front USB cover is open, the front surface is rated for Type 1 enclosure.
Be aware of the following when building this product into an end-use product:
-
The rear face of this product is not approved as an enclosure. When building this product into an end-use product, be sure to use an enclosure that satisfies standards as the end-use product's overall enclosure.
-
Install this product in an enclosure with mechanical rigidity.
-
This product is not designed for outdoor use. UL certification obtained is for indoor use only.
-
Install and operate this product with its front panel facing outward.
CAUTION |
|---|
|
RISK OF BURNING INJURY
Failure to follow these instructions can result in injury or equipment damage.
|
CAUTION