EIO0000004347_01

Starting the Launcher

The Launcher is a utility that you can set up to start programs and settings. The Launcher allows for convenient touch-screen operation by displaying icons for registered various settings.

Download the Harmony P6 and Harmony FP6 Utility from the following URL and install them on the host connected to the product.
www.se.com

After installation, a shortcut icon is created on the desktop. You can start the Launcher from the shortcut icon.

When the Launcher is installed on the host other than Harmony P6:

When the Launcher is installed on Harmony P6:

NOTE:
  • When the Launcher is already installed on the host, the existing Launcher will be overwritten. If you used Edit to customize the Launcher, set up again.

  • When you install this Launcher on a product that has the Launcher pre-installed, please also check the description of utilities in the manual for the host.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?