EIO0000004347_01

System Specifications

For touch input data communication between this product and the host, and for adjustment of the screen display, the communication driver and utilities must be installed on the host.

Download the Harmony P6 and Harmony FP6 Utility from the following URL. The driver will be installed automatically when the utility is installed.
www.se.com

NOTE: Regularly check information for the latest version of the utility and always keep the Launcher up to date.

Operation System

The supported operating systems are listed on the website from which you can download the utilities for this product.

Utility

The utilities you can use on this product are as follows. For more information about each of the following utilities, refer to Launcher.

Launcher:

  • Buzzer

  • Brightness

  • Calibration

  • Front USB

  • Touch Mode

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?