EIO0000004347_01

FP6 System

Displays the version of the utility and firmware for the display.

When this product is connected to the Harmony P6 Panel Type, an icon for selecting the target display is displayed first. When you select an icon, the associated display flashes so you can identify which display to confirm the version.

Front Display: Harmony P6 Panel Type
Extend Display: This product

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?