EIO0000004347_01

Connecting the DC Power Cord

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Remove power before wiring this product’s power terminals.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
  • Use only the specified voltage when operating this product. This product is designed to use 24 Vdc. Always check whether your device is DC powered before applying power.
  • Since this product is not equipped with a power switch, be sure to connect a power switch to the power supply.
  • Be sure to ground this product’s FG terminal.
Failure to follow these instructions will result in death or serious injury.
NOTE:
  • The SG (signal ground) and FG (frame ground) terminals are connected internally in this product.

  • When the FG terminal is connected, be sure the wire is grounded. Not grounding this product can result in excessive electromagnetic interference (EMI).

DC Power Connector: Spring Clamp Terminal Blocks

Connection Wire
+ 24 Vdc
- 0 Vdc
FG Grounded terminal connection to the panel chassis.

How to connect the DC Power Cord

  1. Confirm the power cord is not connected to the power supply.
  2. Crimp a pin terminal properly to the end of each power cable wire.
  3. Push the opening button with a small and flat screwdriver to open the desired pin hole.
  4. Insert each power cord wire into its corresponding hole. Release the opening button to clamp the wire in place.
    NOTE:
    • When using stranded wire, do not short with neighboring wires.

    • When connecting with stranded wires, do not solder the stranded wires.

    • If the wire is not inserted into the FG terminal properly, touch may not respond normally.

    1. Power cord

    2. Opening button

    3. Screw

  5. After inserting all three power cord wires, insert the DC power connector into the power connector on this product.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?