EIO0000004347_01

Maintenance Accessories

Product name

Product number

Description

Installation Gasket

12-inch

HMIZD56

Provides dust and moisture resistance when this product is installed into a solid panel (1 piece)

15-inch

HMIZD57

10-inch Wide

HMIZD55W

12-inch Wide

HMIZD56W

15-inch Wide

HMIZX57W

19-inch Wide

HMIZCWG8W1

22-inch Wide

HMIZCWG9W1

DC Power Supply Connector with fixable screws

HMIZCCNDC1

Connector to connect DC power supply cables (5 pieces/set)

Installation Fastener

HMIZCAF1

 (4 pieces/set)

USB Clamp Type B (1 port)

HMIYFPCLUSB

Clamp to prevent disconnection of USB Type B cable (5 pieces/set)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?