DVI-D Input Interface
DANGER |
|---|
|
ELECTRIC SHOCK AND FIRE
When using the SG terminal to connect an external device
to this product:
Failure to follow these instructions will result in death or serious injury.
|
When this product is connected to the host with the USB Cable accessory, this product receives touch input even if the DVI cable is not connected (and even if the screen is not displayed).
WARNING |
|---|
|
LOSS OF CONTROL
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
|
Pin No. |
Signal name |
Direction |
|---|---|---|
|
1 |
TMDS DATA 2- |
Input |
|
2 |
TMDS DATA 2+ |
Input |
|
3 |
TMDS DATA 2 SHIELD (SG) |
– |
|
4 |
NC |
– |
|
5 |
NC |
– |
|
6 |
DDC Clock |
Input |
|
7 |
DDC Data |
Input/Output |
|
8 |
NC |
– |
|
9 |
TMDS DATA 1- |
Input |
|
10 |
TMDS DATA 1+ |
Input |
|
11 |
TMDS DATA 1 SHIELD (SG) |
– |
|
12 |
NC |
– |
|
13 |
NC |
– |
|
14 |
+5 V |
+5 V power input for DDC |
|
15 |
SHIELD (SG) |
– |
|
16 |
Hot Plug Detect |
Output |
|
17 |
TMDS DATA 0- |
Input |
|
18 |
TMDS DATA 0+ |
Input |
|
19 |
TMDS DATA 0 SHIELD (SG) |
– |
|
20 |
NC |
– |
|
21 |
NC |
– |
|
22 |
TMDS CLOCK SHIELD (SG) |
– |
|
23 |
TMDS CLOCK+ |
Input |
|
24 |
TMDS CLOCK- |
Input |
|
Shell |
FG |
Frame Ground (Common with SG) |
Recommended jack screw is #4-40 (UNC).
For noise-free operation, use the recommended DVI-D cable. Refer to Accessories.
Display Resolution
The supported refresh rate is 60 Hz.
|
Model |
Recommended resolution |
Horizontal frequency (Hz) |
Vertical frequency (Hz) |
Pixel clock (MHz) |
|---|---|---|---|---|
| HMIFP6600TMD/HMIFP6700TMD |
1,024 x 768 (XGA) |
48.363 |
60.004 |
65.000 |
| HMIFP6500WCD/HMIFP6600WCD |
1,280 x 800 (WXGA) |
49.306 |
59.910 |
71.000 |
| HMIFP6700WCD |
1,366 x 768 (FWXGA) |
48.000 |
60.000 |
72.000 |
| HMIFP6800WCD/HMIFP6900WCD |
1,920 x 1,080 (FHD) |
67.500 |
60.000 |
148.500 |
If you change to a resolution that is not recommended, the display may appear blurry and unclear.
|
Resolution |
Horizontal frequency (Hz) |
Vertical frequency (Hz) |
Pixel clock (MHz) |
|---|---|---|---|
|
640 x 480 (VGA) |
31.469 |
59.940 |
25.175 |
|
800 x 600 (SVGA) |
37.879 |
60.317 |
40.000 |
|
1,024 x 768 (XGA) |
48.363 |
60.004 |
65.000 |
DANGER
WARNING