JYT97577–01

Modbus Communication Interface Module (IFM)

This module, required for connection to the network, contains the Modbus address (1 to 99) declared by the user using the two rotary switches on the front of the unit. It automatically adapts (baud rate, parity) to the Modbus network in which it is installed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.