PHA6516400-06

Meter wiring

The meter is equipped with 2 tariff functions, which is configured through Modbus communication between terminals 23 and 24.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?