PHA6516400-06

Setting up registers

To add or remove registers to/from automatic scroll, follow these steps:
  1. Scroll to the register * that you would like to add or remove.
  2. Hold the button for 5 seconds to add or remove the register.
  3. The LCD displays OK in or OK out .
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.