PHA6516400-06

DIN mount energy meter

A Neutral in (4) and Neutral out (6)
B Pulse output (20 and 21)
C Button
D LCD display
E Modbus communication (23 and 24)
F Line in (1) and Line out (3)
G Energy flow LED indicator
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?