PHA6516400-06

Meter overview

The iEM2050 series meter is a single phase meter which measures the forward and reverse energy.

All meters in the iEM2050 series range comply with Class 1 or Class B accuracy standards and feature high quality, reliability and affordability in a compact and easy to install format.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.