PHA6516400-06

Button functions

Action Button function

Press the button for less than 3 seconds

To enable scroll.

NOTE: After 30 seconds of no interaction the meter goes back to automatic scroll mode.

Press the button for 3 seconds

To enter the next menu/to go back to previous menu.

To confirm parameter settings.

Hold the button for more than 5 seconds

To add or remove from the automatic scroll mode.

To enter program mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.