iEM2050 meter models
Meter models
| Model | Commercial reference | Description |
|---|---|---|
|
iEM2050 |
A9MEM2050 |
Class 1 accuracy as per IEC 62052-11 and IEC 62053-21 |
|
iEM2055 |
A9MEM2055 |
Class 1 accuracy as per IEC 62052-11 and IEC 62053-21 Class B as per EN 50470-1/3 MID compliance |
|
NOTE: These
meters use a two-wire Modbus connection. Ensure that the Modbus transmission
line does not exceed 10 meters to maintain reliable communication.
NOTE: When integrating these meters with three-wire Modbus equipment
(signals + 0V common), connect the meter through a branch circuit
using an LU9GC3 splitter and a VW3A8306D30 cable. This configuration
ensures proper signal referencing and communication reliability.
|
||