PHA6516400-06

Tariff

Command Number

Action
(R/W)

Size

Type

Unit

Range

Description

2008

W

1

UInt16

(Reserved)

W

1

UInt16

1, 2

Tariff:

  • 1 = T1
  • 2 = T2

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.