PHA6516400-06

Setting up combination code

The meter allows you to display the total energy (usage) based on the combination code. The combination code is in accordance with different calculation methods as shown below:
Code Total (active) energy
C-01 Forward only
C-04 Reverse only
C-05 Forward + Reverse
C-06 Reverse - Forward
C-09 Forward - Reverse
C-10 Forward - Reverse
To change the combination code, follow these steps:
  1. Scroll with the button to Program mode 3 (PM0dE3).
  2. Hold the button for 3 seconds to enter the menu.
  3. Enter the 4 digit password: scroll with the button and select each digit 0 – 9, hold the button for 3 seconds to confirm each digit. Default password is 0000.
  4. Scroll to LCD combination code (C-xx) page.
  5. Hold the button for 5 seconds to enter program mode.
  6. When the value starts blinking: select 01/04/05/06/09/10.
  7. Hold the button for 3 seconds to confirm the new setting.
  8. The LCD displays OK when the setting is confirmed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.