System
| Address | Register | Action | Size | Type | Units | Description |
|---|---|---|---|---|---|---|
|
0x001E |
31 |
R |
20 |
UTF8 |
- |
Meter name |
|
0x0032 |
51 |
R |
20 |
UTF8 |
- |
Meter model |
|
0x0046 |
71 |
R |
20 |
UTF8 |
- |
Manufacturer |
|
0x005A |
91 |
R |
1 |
UInt16 |
- |
Meter code |
|
0x0082 |
131 |
R |
2 |
UInt32 |
- |
Serial number |
|
0x0088 |
137 |
R |
5 |
UTF8 |
- |
Hardware revision in x.x.x format (for example, 1.0.0) NOTE: The
first number is the major version, the second number is the minor
version, and the third number is normally not used.
|
|
0x0665 |
1638 |
R |
1 |
UInt16 |
- |
Present firmware version |