PHA6516400-06

Setting up Modbus ID

The Modbus ID can be set from 001 to 247. The default Modbus ID is 001.
To change the Modbus ID, follow these steps:
  1. Scroll with the button to Program mode 2 (PM0dE2).
  2. Hold the button for 3 seconds to enter the menu.
  3. Scroll to LCD Modbus ID (MOd Id xxx) page.
  4. Hold the button for 5 seconds to enter program mode.
  5. When the value starts blinking: select 3 digits (001 – 247).
  6. Hold the button for 3 seconds to confirm each digit.
  7. The LCD displays OK when the setting is confirmed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.