PHA6516400-06

Resetting power down counter

The power down counter registers the number of times the meter has been turned off.
To reset the power down counter, follow these steps:
  1. Scroll with the button to Program mode 3 (PM0dE3).
  2. Hold the button for 3 seconds to enter the menu.
  3. Enter the 4 digit password: scroll with the button and select each digit 0 – 9, hold the button for 3 seconds to confirm each digit. Default password is 0000.
  4. Scroll to LCD power down counter (PWEr C xxxx) page.
  5. Hold the button for 5 seconds to enter program mode.
  6. When the value starts blinking: hold the button for 3 seconds to reset.
  7. The LCD displays OK when the power down counter (PWEr C xxxx) is reset.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.