PHA6516400-06

Meter setup and status

Address Register Action Size Type Units Description

0x0725

1830

R

1

UInt16

-

Power on off counter

0x07DE

2015

R

1

UInt16

-

Number of phases (always 1)

0x07DF

2016

R

1

UInt16

-

Number of wires (always 2)

0x07E0

2017

R

1

UInt16

-

Power system (always 0 = 1PH2W L-N)

0x07E1

2018

R

1

UInt16

Hz

Nominal frequency

0x07E4

2021

R

2

Float32

A

Meter Amps

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?