PowerPacT™ Automatic Switches

Class 0612 / Refer to Catalog 0612CT0101

Automatic Switches

Automatic molded case switches open instantaneously at a factory preset magnetic trip point, calibrated to protect only the molded case switch itself, when it is subjected to high fault currents. The trip point is nonadjustable and provides no overload or low level fault protection.

Molded case switches open when the handle is switched to the OFF position or in response to an auxiliary tripping device such as a shunt trip.

All molded case switches will accept the same lugs and accessories as equivalent thermal-magnetic circuit breakers, with the exception of Q-frame switches which do not have electrical accessories available.

Automatic molded case switches are UL Listed per UL 489 and are CSA Certified.

Q-Frame (240 Vac) PowerPacT™ Automatic Molded Case Switches

Circuit Breaker

Poles

Ampere Rating

J Interrupting Rating

Wire Range

Cat. No.

Trip Point

Q-Frame[1]

2

225 A

QBL22000S22

4500 A

4 AWG–300 kcmil

3

225 A

QBL32000S22

4500 A

Footnotes

  1.  Withstand rating of 10 kA at 240 Vac.
Feedback