Mechanical Lug Information
Mechanical Lug Kits
Mechanical Lug Kit Information
|
Circuit Breaker Application |
(Number of Wires
Per Lug) |
Cat. No. |
Lugs |
|||
|---|---|---|---|---|---|---|
|
Standard |
Ampere |
Optional |
Ampere |
|||
|
Al Lugs for Use with Al or Cu Wire |
||||||
|
Q4, LA, LH |
125–400 A |
— |
— |
(1) 1 AWG–600 kcmil or |
1 |
|
|
— |
— |
Q4, LA, LH |
125–400 A |
(1) 350–750 kcmil |
1 |
|
|
Cu Lugs for Use with Cu Wire Only [2] |
||||||
|
— |
— |
Q4, LA, LH |
125–400 A |
(1) 1 AWG–600
kcmil Cu or |
1 |
|