Field-Installable Accessories

Field-Installable Electrical Accessories

Auxiliary Switch
Contact Configuration

1A Alarm Switch
Configuration

1B Alarm Switch
Configuration

Undervoltage Trip
Wiring Diagram

Shunt Trip
Wiring Diagram

Complete field-installable accessory catalog number by inserting suffix from Factory-Installed Electrical Accessories between the parentheses in the catalog numbers shown in the table below. (Example: LA11212)

Field-Installable Accessories for Thermal-Magnetic and Electronic Trip Circuit Breakers

Circuit Breaker

Shunt Trip

Ground-Fault
Shunt Trip [1]

Undervoltage Trip

Auxiliary Switches

Alarm Switch

Miniature Circuit Breakers
EH and EH-PL

Factory-Installed Only

Not Available

Not Available

Factory-Installed Only

Factory-Installed Only

LA, LH
Series 4 [2]

LA1(  )

LA1G

LA1 (  )

LA1(  )

Factory-Installed Only Right Pole

Q4

LA1(  )

LA1G

LA1 (  )

LA1(  )

Factory-Installed Only Right Pole

Accessory Mounting Locations

LA, LH, Q4 Series 4 circuit breakers or newer = Field-installable accessories

Both accessory ports will accept shunt trips, UVRs and auxiliary switches. Alarm switches are factory installable only (right pole). Maximum of one device per port.

Footnotes

  1. Used with obsolete GP Ground-Censor™ system or add-on ground-fault modules.
  2. With LA and LH top-feed circuit breakers (suffix MT, I-Line jaws on OFF end) all accessories must be factory installed.
Feedback