Pricing Procedure Examples

Class 1630

NQOD Merchandised Pricing Procedure

1. List circuit breakers required, either plug-on or bolt-on. See appropriate pages for catalog numbers.

2. Determine equivalent number of pole spaces required.

3. Select proper main lugs interior or main lugs interior and main circuit breaker adapter kit based on equivalent number of poles and ampere rating from appropriate page. Interiors include solid neutral and are field convertible to top feed.

4. Select enclosure from appropriate page.
Type 1—Select box and front catalog number corresponding to interior catalog number. Types 3R, 5, 12—Select enclosure, front included.

5. For complete price, add the component prices. Include panelboard accessories.

6. Apply appropriate discount schedule.

Was this helpful?