PHA5538902-05

Meter overview

The PM1125H / PM1110H meter offers comprehensive 3-phase electrical instrumentation and load management facilities in a compact and rugged package.

The PM1125H / PM1110H meter offers value for the demanding needs of your energy monitoring and cost management applications. Meters in the series range comply with Class 0.5S / Class 0.2 / Class 1.0 accuracy standards and feature high quality, reliability and affordability in a compact and easy to install format.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?