PHA5538902-05

Panel meter

LED indicators

The LED indicators alert or inform you of meter activity or status. Refer to the following image for the various LED indicators the meter provides.

A Energy pulsing LED (Red)
B Heartbeat / serial communications LED (Green)

Rear wiring

The meter provides current and voltage inputs along with other wiring options.Refer to following image for various wiring options the meter provides.

A Input voltage terminals (V1, V2, V3, VN)
B Auxiliary power supply (control power) terminals (L1, L2)
C RS-485 communications terminals (D1+, D0-)
D Input current terminals (I1+, I1- , I2+ , I2- , I3+ , I3-)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?