PHA5538902-05

Tot INTG

Applicable for METSEPM1125HCL1LVD / METSEPM1125HCL5LDD

To view tot INTG parameters:

  1. From the Home page, use Up or Down button to navigate to Tot INTG.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next Tot INTG parameter.
  4. Press Left button to exit.

Name on display

Description

d. wh

Displays the delivered active energy

d. VRh

Displays the delivered reactive energy

d. VAh

Displays the delivered apparent energy

d. Rh

Displays the delivered run hours, for example hhhhhh:mm

NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.

R. wh

Displays the received active energy

R. VRh

Display the received reactive energy

R. VAh

Displays the received apparent energy

R. Rh

Displays the received run hours, for example hhhhhh:mm

NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.

t. wh

Display the total active energy

t. VRh

Displays the total reactive energy

t. VAh

Displays the total apparent energy

t. Rh

Displays the total run hours, for example hhhhhh:mm

NOTE: Run Hours are displayed with 6 digit Hours and 2 digit Minutes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?