PHA5538902-05

Instantaneous

The meter provides highly accurate 1-second measurements, average values, including true RMS, per phase and total for:

Applicable for PM1125H

  • Per-phase and average voltage (line-to-line, line-to-neutral)

  • Per-phase and average current, and neutral current (calculated)

  • Per-phase and average power factor

  • Per-phase and total power (VA, W, VAR)

  • System frequency

  • Revolutions per minute (RPM)

  • Unbalance (voltage, current)

  • Load percentage

  • Phase angle, per-phase (between voltage and current)

Applicable for PM1110H

  • Per-phase and average power factor

  • Per-phase and total power (VA, W, VAR)

  • Revolutions per minute (RPM)

  • Unbalance (voltage, current)

  • Load percentage

  • Phase angle, per-phase (between voltage and current)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?