PHA5538902-05

Meter configuration

Meter configuration can be performed through the display (if your meter is equipped with one) or meter webpages or ION Setup .

ION Setup is a meter configuration tool that can be downloaded for free at www.se.com .

See the ION Setup online help or in the ION Setup device configuration guide. To download a copy, go to www.se.com and search for ION Setup device configuration guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?