PHA5538902-05

Editing setup parameters

The following steps describe how to edit parameters in setup mode.
  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Use Up or Down button to navigate to Set.
  4. Press OK.
  5. Enter password. Default password is 0000.
  6. Press OK.
  7. Press the Up or Down button to select a parameter to edit. The selected parameter flashes the digit, value, or decimal point that is required to be set (the meter automatically determines which option to flash for editing, depending on the parameter).
  8. Increase or decrease the digit value, move the decimal point, or select a value from a pre-programmed list using the Up or Down button.
  9. Press OK after making the required changes.
  10. Press Left button.
  11. Select Yes to save your settings.
NOTE: Select No to exit setup mode without saving any settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?