PHA5538902-05

RMS page

To view RMS parameters:

NOTE: The display shows different RMS parameters based on the meter model.
NOTE: Favourite page is not available in PM1110H.
  1. From the Home (RMS) page, use Up or Down button to navigate to RMS.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next RMS parameter.
  4. Press Left button to exit.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?