PHA5538902-05

INTG page

To view INTG parameters:

  1. From the Home page, use Up or Down button to navigate to INTG.
  2. Press OK.
  3. Press the Up or Down button to navigate to the next INTG parameter.
  4. Press Left button to exit.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?