PHA5538902-05

Front panel

The front panel contains the following indicators and controls:

  • Eight-segment LED display: Three rows of alphanumeric displays, four digits each, display three RMS parameters simultaneously or one energy parameter. The displayed readings update every second.

  • Analog load bar: Unique indication of % load with respect to the full scale (FS).

  • Indicators: Each row displays Kilo, Mega (Kilo + Mega = Giga) indicators, and a negative (-) indicator.

  • Keys: Four smart keys to scroll through the display pages.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?