PHA5538902-05

Meter types

The meter is available in one physical form factor.
Commercial reference Features description

METSEPM1125HCL10RS

  • Class 1 panel mount meter with RS-485

  • Integrated display

METSEPM1125HCL10RD

METSEPM1110HCL1

METSEPM1125HCCL1

  • Class 1 panel mount meter with RS-485

  • Integrated display

  • Conformal coating as per UL746E standard

METSEPM1125HCCL05

  • Class 0.5S panel mount meter with RS-485

  • Integrated display

  • Conformal coating as per UL746E standard

METSEPM1110HCL05

  • Class 0.5S panel mount meter with RS-485

  • Integrated display

METSEPM1125HCL05RD

METSEPM1125HCL02RD

  • Class 0.2 panel mount meter with RS-485

  • Integrated display

METSEPM1125HCL1LVD

  • Class 1 panel mount meter with RS-485

  • low voltage DC with Integrated display

METSEPM1125HCL5LVD

  • Class 0.5 panel mount meter with RS-485

  • low voltage DC with Integrated display

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.