PHA5538902-05

Overview

You can configure the meter’s setup parameters through the meter’s RS-485 communications port.

The meter is factory-configured with default RS-485 communications port settings. You must modify the default settings before connecting the meter to your RS-485 network. To configure the RS-485 port, you need:

  • ION Setup

NOTE: Remote meter setup is applicable only for meter models supporting RS-485 communication.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?