PHA5538902-05

Display screen menu tree

Use the menu tree to navigate to the setting you want to view.

Parameter navigation

The following image summarizes the RMS parameters under meter:

NOTE: The display shows different RMS parameters based on the meter model.
NOTE: Favourite page is not available in PM1110H.

Favourite page

The meter allows you to select 3 parameters and arrange them in required order to be displayed in favourite page. These parameters can be selected only through communication and are based customer requirements. Some parameter logs are of utmost importance and navigating to those parameters takes time. For ease of navigation and accessibility, the meter allows you to chose 3 parameters and lock the page for easy reading. The selectable parameters are:

  • V L-L

  • V L-N

  • A

  • F

  • W

  • PF

  • VA

  • VAR

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?