Configure Client Machine

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

Perform the steps in this section to configure a client machine to accept updates from the SDE geodatabase via the Web Service. Refer to the appropriate Geodatabase Replication ReadMe version for hardware and software requirements.

Multiple Replication Clients: If you have multiple replication client machines, you may wish to disseminate a single client configuration file rather than configuring each machine individually. You can configure one ReplicationConsole.exe.config file and copy it to a shared network drive that allows access from client machines.

QR code for this page

Was this helpful?