0611IB1302-08

Standard Dataset

Description

The standard dataset contains the most useful information of each IMU module in one convenient table. The standard dataset is available in the registers 32000 to 32341. It can be read with three read requests.

Each IMU module updates the values in the dataset registers on a regular basis.

The response time of requests to standard dataset registers is shorter than the response time of requests to device registers. Therefore, it is recommended to read the standard dataset registers instead of device registers, to improve the overall performance of the system Modbus Programming Recommendations.

The standard dataset can be used with:

  • the IFE Ethernet interface for one circuit breaker

  • the IFE Ethernet switchboard server

  • the IFM Modbus-SL interface for one circuit breaker