Circuit Breaker Status
Circuit Breaker Status
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0232 |
563 |
R |
– |
– |
INT16U |
– |
A/E |
– |
Circuit breaker status register |
|
0 |
OF input status 0 = The circuit breaker is open. 1 = The circuit breaker is closed. |
||||||||
|
1 |
SD input status 0 = The circuit breaker is not tripped. 1 = The circuit breaker is tripped due to electrical default or shunt trip or push-to-trip. |
||||||||
|
2 |
SDE input status 0 = The circuit breaker is not tripped on electrical default. 1 = The circuit breaker is tripped due to electrical fault (including ground-fault test). |
||||||||
|
– |
3–15 |
Reserved (forced to 0) |
Communicating Motor Operator Status
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0233 |
564 |
R |
– |
– |
INT16U |
– |
A/E |
– |
Communicating motor operator status register |
|
0 |
Motor operator 0 = not available 1 = available |
||||||||
|
1 |
Manu/auto mode 0 = manu 1 = auto |
||||||||
|
2 |
Last command 0 = last command succeeded 1 = last command failed |
||||||||
|
3 |
Enable automatic reset 0 = automatic reset is not enabled. 1 = automatic reset is enabled. |
||||||||
|
4 |
Enable reset even if SDE 0 = reset is not enable if the circuit breaker is tripped on electrical default. 1 = reset is enabled even if the circuit breaker is tripped on electrical default. |
||||||||
|
5 |
Local/Remote mode selected in the FDM121 display menu. 0 = Remote mode (default value), the communicating motor operator is controlled through a Modbus command only. 1 = Local mode, the communicating motor operator is controlled through the FDM121 display menu only. |
||||||||
|
– |
6–15 |
Reserved (forced to 0) |