0611IB1302-08

List of IO Module Commands

List of Commands

There are two types of command:

  • generic commands which work independently of the application selected.

  • application commands which are dedicated to an application. A command is only valid if the related application is configured.

The following table lists the available IO module commands, their corresponding application, command codes and user profiles. Follow the command execution procedures accordingly. Executing a Command

Application

Command

Command code

User profile

Generic

Change output state

1672

Administrator or Operator

Generic

Reset IO module alarms

41099

Administrator or Operator

Generic

Enable/Disable simple commands

41100

Administrator or Operator

Generic

Acknowledge latched output

41102

Administrator or Operator

Generic

Reset analog input minimum/maximum values

42890

Administrator or Operator

Cradle and drawer management

Preset cradle/drawer counters

41352

Administrator or Operator

Cradle and drawer management

Preset cradle/drawer regrease timers

41353

Administrator or Operator

Light control

Light control

42120

Administrator or Operator

Load control

Load control

42376

Administrator or Operator

Pulse counter management

Preset input pulse counter

42888

Administrator or Operator

Cooling system

Preset switchboard temperature threshold counter

42889

Administrator or Operator

IO Module Error Codes

The error codes generated by the IO module are the generic error codes Result of the Command.