0611IB1302-08

Schematics with PowerPact H-, J-, and L-Frame Circuit Breakers

General Description

Depending on the configuration of the PowerPact H-, J-, and L-frame circuit breaker, connect the IFE interface to the circuit breaker using one of the following configurations:

  • Connection of the IFE interface to the MicroLogic trip unit

  • Connection of the IFE interface to the BSCM module

  • Connection of the IFE interface to the BSCM module and to the MicroLogic trip unit

For more information, refer to the ULP System User Guide.

ULP Connection

NOTICE
HAZARD OF EQUIPMENT DAMAGE
  • Never connect an Ethernet device to a RJ45 ULP port.
  • The RJ45 ULP ports of IFE interface are for ULP modules only.
  • Any other use can damage the IFE interface or the device connected to the IFE interface.
  • To check if a ULP module is compatible with the RJ45 ULP ports of IFE interface, refer to the ULP System User Guide.
Failure to follow these instructions can result in equipment damage.

All connection configurations require the NSX cord. The insulated NSX cord is mandatory for system voltages greater than 480 Vac.

When the second RJ45 ULP port is not used, it must be closed with an ULP line termination.

A NSX cord or RJ45 ULP cord

B ULP line termination

Connection of the IFE Interface to the MicroLogic Trip Unit

A IFE Ethernet interface for one circuit breaker

B ULP line termination

C NSX cord

D MicroLogic trip unit

Connection of the IFE Interface to the BSCM Module

A IFE Ethernet interface for one circuit breaker

B ULP line termination

C NSX cord

D BSCM breaker status control module

Connection of the IFE Interface to the BSCM Module and to the MicroLogic Trip Unit

A IFE Ethernet interface for one circuit breaker

B ULP line termination

C NSX cord

D BSCM breaker status control module

E MicroLogic trip unit

Connection of the IFE Interface to a Circuit Breaker for System Voltage Greater Than 480 Vac

A IFE Ethernet interface for one circuit breaker

B ULP line termination

C RJ45 ULP cord

D Insulated ULP module for system voltage greater than 480 Vac

E Insulated ULP cord for system voltage greater than 480 Vac

F Connector for PowerPact H-, J-, and L-frame Circuit Breakers internal connection