Trip History
General Description
The trip history registers describe the last 17 encountered trips. The trip history format corresponds to a series of 17 records. Each record is composed of 7 registers describing one trip.
The trip history registers return 32768 (0x8000) when they are not used.
Trip Record Number
A read request of 7x(n) registers is necessary to read the last n trip records, where 7 is the number of registers for each trip record.
For example, a read request of 7 x 4 = 28 registers is necessary to read the last 4 trip records of the trip history:
-
The first 7 registers describe the first trip record (most recent trip).
-
The next 7 registers describe the second trip record.
-
The last 7 registers describe the third trip record.
-
The last 7 registers describe the fourth trip record.
|
Address |
Register |
Description |
|---|---|---|
|
0x238B–0x2391 |
9100–9106 |
Trip record 1 (most recent trip) |
|
0x2392–0x2398 |
9107–9113 |
Trip record 2 |
|
0x2399–0x239F |
9114–9120 |
Trip record 3 |
|
0x23A0–0x23A6 |
9121–9127 |
Trip record 4 |
|
0x23A7–0x23AD |
9128–9134 |
Trip record 5 |
|
0x23AE–0x23B4 |
9135–9141 |
Trip record 6 |
|
0x23B5–0x23BB |
9142–9148 |
Trip record 7 |
|
0x23BC–0x23C2 |
9149–9155 |
Trip record 8 |
|
0x23C3–0x23C9 |
9156–9162 |
Trip record 9 |
|
0x23CA–0x23D0 |
9163–9169 |
Trip record 10 |
|
0x23D1–0x23D7 |
9170–9176 |
Trip record 11 |
|
0x23D8–0x23DE |
9177–9183 |
Trip record 12 |
|
0x23DF–0x23E5 |
9184–9190 |
Trip record 13 |
|
0x23E6–0x23EC |
9191–9197 |
Trip record 14 |
|
0x23ED–0x23F3 |
9198–9204 |
Trip record 15 |
|
0x23F4–0x23FA |
9205–9211 |
Trip record 16 |
|
0x23FB–0x2401 |
9212–9218 |
Trip record 17 (oldest trip) |
Trip Record
A read request of 7 registers is necessary to read a trip record.
The order and the description of the trip record registers are the same as that of the trip record 1:
|
Trip Record 1 (Most Recent Trip) |
||||||||
|---|---|---|---|---|---|---|---|---|
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|
0x238B |
9100 |
R |
1 |
– |
INT16U |
0–65535 |
A/E |
Trip code (see next paragraph) |
|
0x238C– 0x238E |
9101– 9103 |
R |
– |
– |
ULP DATE |
– |
A/E |
Date and time of event (trip or acknowledge. Data Type: ULP DATE |
|
0x238F |
9104 |
R |
1 |
– |
INT16U |
1–2 |
A/E |
Event type MSB = 0 (reserved) Event occurrence: LSB = 1 Event completion: LSB = 2 |
|
0x2390 |
9105 |
R |
1 |
– |
INT16U |
0–5 |
A/E |
Faulty phase 0 = failure (no faulty phase) 1 = phase A 2 = phase B 3 = phase C 4 = phase N 5 = phase A B C (motor application, ground-fault) |
|
0x2391 |
9106 |
R |
1 |
A |
INT16U |
0–65535 |
A/E |
Interrupted current (peak) (1) |
|
(1) Measurement depends on the application:
|
||||||||
Trip Codes
|
Trip Code |
Description |
|---|---|
|
1000 (0x03E8) |
Long-time protection Ir |
|
1001 (0x03E9) |
Short-time protection Isd |
|
1002 (0x03EA) |
Instantaneous protection Ii |
|
1003 (0x03EB) |
Ground-fault protection Ig |
|
1004 (0x03EC) |
Reserved |
|
1005–1009 (0x03ED–0x03F1) |
Reserved |
|
1010 (0x03F2) |
Integrated instantaneous protection |
|
1011 (0x03F3) |
STOP (trip unit internal failure) |
|
1012 (0x03F4) |
Reserved |
|
1013–1031 (0x03F5–0x0407) |
Reserved |
|
1032 (0x0408) |
Unbalance motor protection |
|
1033 (0x0409) |
Jam motor protection |
|
1034 (0x040A) |
Underload motor protection |
|
1035 (0x040B) |
Long-start motor protection |
|
1036 (0x040C) |
Reflex tripping protection |