0611IB1302-08

BSCM Module Identification

Product Identification

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x0226

551

R

INT16U

15149

A/E

Product identification = 15149 for the BSCM module

BSCM Module Identifier

The BSCM module serial number is composed of a maximum of 11 alphanumeric characters with the following format: PPYYWWDnnnn.

  • PP = plant code

  • YY = year of fabrication (05–99)

  • WW = week of fabrication (01–53)

  • D = day of fabrication (1–7)

  • nnnn = sequence number (0001–9999)

A read request of 6 registers is necessary to read the BSCM module serial number.

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x0227

552

R

OCTET STRING

A/E

‘PP’

0x0228

553

R

OCTET STRING

05–99

A/E

‘YY’

0x0229

554

R

OCTET STRING

01–53

A/E

‘WW’

0x022A

555

R

OCTET STRING

1–7

A/E

‘Dn’

0x022B

556

R

OCTET STRING

00–99

A/E

‘nn’

0x022C

557

R

OCTET STRING

01–99

A/E

‘n’ (the NULL character ends the serial number)